Technical FAQs

Ask a Question

MPPT80: What size cable can this controller accept?

Issue:
Not sure what size cable the MPPT 80 Solar Charge Controller can accept.

Product Line:
MPPT 80 600

Environment:
MPPT 80 new installation

Resolution:
Maximum and Minimum Wire Size in Conduit
-#6 AWG to #14 AWG (13.5 to 2.5 mm2)

Maximum and Minimum Wire Size Rating of PV Terminal Block
-#6 AWG to #14 AWG (13.5 to 2.5 mm2)

Maximum and Minimum Wire Size Rating of Battery Terminal Block
-#2 AWG to #14

Cause:
The manual is either not available or the customer is unable to find the information in the Installation Guide.
Was this helpful?
What can we do to improve the information ?