Technical FAQs

Ask a Question

How many IG2000PG's and IG2000CBM's remotes can be connected to an IG6M LIM ?

Issue:
How many IG2000PG's and IG2000CBM's remotes can be connected to an IG6M LIM ?

Product Line:
Medical Products

Environment:
Application

Cause:
Clarification

Resolution:
The IG6 LIM's standard is (4) IG2000P and (2) IG2000CBM remotes per LIM. With a 12VDC Power supply they can add an addtl (4) IG2000P.
The IG2000P 's have a 50mA Current draw each . 2 addtl IG2000CBM's can be added to LIM and consume 100mA each. No testing has been done using (4) IG2000CBM's on one LIM, but as long as distance is short , it can be accomplished with the use of a Power supply as well
Was this helpful?
What can we do to improve the information ?