Technical FAQs

Ask a Question

Video: How to install the EIK031 or EIK032 interlock kit in an F-series safety switch

Issue:
Installation Instructions on EIK interlock kits
 
Product Line:
Electrical Interlock Kits
 
Environment:
Heavy Duty Safety Switches
 
Resolution:
 
You would fit the lower tab on the kit into the tab on the safety switch handle mechanism. Once that is lined up, you would rock the interlock kit forward until the square tab on the handle mechanism fits through the square hole on the interlock kit, and the mounting hole on the kit lines up with the mounting hole in the safety switch. You would then install the mounting screw provided with the kit. See the below video or attached instruction bulletin for further installation help.

[video placeholder]
 
 
Was this helpful?
What can we do to improve the information ?