Technical FAQs

Ask a Question

What is the mounting height for Powerpact B-Frame I-Line breakers?

Issue:
What is the mounting height for Powerpact  B frame I-Line breakers? 

Product Line:
Powerpact B-Frame

Resolution:
Powerpact B frame I-Line breakers require the folowing mounting space based on the number of poles:

1-Pole = 1.5 inches
2-Pole = 3 inches
3-Pole = 4.5 inches
 

Keywords

Powerpact B frame circuit breakers, width, wide, Powerpact B frame, BDA, BGA, BJA, BKA, I-Line mounting height
Was this helpful?
What can we do to improve the information ?