Technical FAQs

Ask a Question

What is the number of operations for switching for P frame breaker?

Issue:
Number of operations for switching for P frame breaker.

Product Line:
Powerpact P-Frame

Environment:
All

Cause:
Customer is unable to find the information for the number of operations for switching for P frame breaker.

Resolution:
The endurance of the Powerpact P frame is 2500 mechanical operations. 500 of which is with full load current and 2000 is without current. This also applies to Powerpact M and R frames as well.

 
Was this helpful?
What can we do to improve the information ?