Technical FAQs

Ask a Question

How do the Vigirex ground-fault relays trip a circuit breaker?

Issue:  
How does the Vigirex relay affect the circuit breaker's position?

Product line:  
Molded case circuit breakers

Environment:  
VigirexTM Ground-Fault Relays

Resolution:  
The Vigirex relay sends an output signal to a shunt trip or under-voltage release installed in the associated circuit breaker.  See the Vigirex System Catalog 0972CT0401 for more details.  
Was this helpful?
What can we do to improve the information ?