Technical FAQs

Ask a Question

Are there any BAC communication options for NEMA combination starters?

Issue:
Are there any BAC communication options for NEMA combination starters?

Product Line:
NEMA Starters - GIC Product

Environment:
US Product

Cause:
Product Selection

Resolution:
There are no BAC interface options for 8538 units.  Communication options are available via TeSys T overload unit, current protocols include Modbus, Ethernet TCP/IP (Ethernet IP and Modbus TCP), CANopen, DeviceNet, and Profibus.
Was this helpful?
What can we do to improve the information ?