Technical FAQs

Ask a Question

What does X and Y represent on a circuit breaker drawing?

Issue:
Circuit Breaker CAD drawings sometimes have an X and Y axis on the front view of the breaker. The X and Y axis also sometimes appear on the pdf version of the drawing. What does X and Y represent?

Product Line:
Circuit Breakers

Environment:
CAD and related pdf drawings of circuit breakers

Resolution:
On circuit breaker CAD drawings, the X and Y axis represent the center point of the circuit breaker. The corresponding pdf version of the drawing often will show the same X and Y center point (reference the drawing below.)
Was this helpful?
What can we do to improve the information ?