Technical FAQs

Ask a Question

Unable to Enable Enhanced AC Support on SW Series Inverter

Issue:
User is using the Combox to enable Enhanced AC Support on SW Series Inverter and getting the error "The value could not be changed".
User already have the charge controller in the Xanbus network ready for Enhanced AC Support.


Product Line:
SW Series Inverter

Environment:
SW Series Inverter

Cause:
Combox not allowing SW Settings update due to the unit operating.

Resolution:
Configure the SW Inverter into StandBy Mode and make the changes in Combox.
Was this helpful?
What can we do to improve the information ?