Technical FAQs

Ask a Question

Can the ComBox network settings be changed via Modbus registers?

Issue: 
Customer is contacting us confirming if he could change his IP address via Modbus.

Product Line: 
Conext XW+ 865-6848 865-5548

Environment: 
Production Information

Resolution:
No, network settings cannot be changed via Modbus.

Cause: 
The IP address details and configuration parameters are not accessible through Modbus for the Conext ComBox. The only Modbus registers that can be monitored and/or written to are posted the Modbus menu map.
Was this helpful?
What can we do to improve the information ?