Technical FAQs

Ask a Question

Where can I find the size of the nut for my ground bolt for my CLNA unit?

Issue:
Customer is working on a new installation and is looking for the nut size for the grounding bolt (earthing terminal).

Product Line:
CLNA18000 CLNA25000

Environment:
Installation Support

Resolution:
Bolt size is M6 NUT.

Cause:
All the nut sizes can be found on the quick start guide, linked below.

http://cdn.solar.schneider-electric.com/wp-content/uploads/2015/07/conext-cl-18-25-na-quick-start-guide-990-9688a-001_rev02_eng.pdf
Was this helpful?
What can we do to improve the information ?