Technical FAQs

Ask a Question

U-Line Coordination

Issue:
What coordination level is the TeSys U by itself?

Product Line:
U-Line Starters - GIC Product

Environment:
US Product

Cause:
Product Specification

Resolution:
For a single basic starter consisting of base LUB12/32, control unit LUCxxx, and line phase barrier LU9SP0, the U-Line has a total coordination level.  Due to its "all in one" construction, TeSys U cannot suffer from contacts welding, which is acceptable for coordination level 2.  Thus the U-Line reaches what we call "total coordination" which is the highest continuity of service for our customers.
Was this helpful?
What can we do to improve the information ?