Technical FAQs

Ask a Question

Maximum Number of Pushbuttons for Wireless Access Point

Issue:
What is the maximum number of pushbuttons which can be programmed to the wireless access point?

Product Line:
Wireless Pushbuttons - GIC Product

Environment:
US Product

Cause:
Product Specifications

Resolution:
A user can program up to 60 buttons for 60 discreet outputs.
Was this helpful?
What can we do to improve the information ?