Technical FAQs

Ask a Question

AK5 Tap-offs

Issue:
Do the AK5 busbars come with tap-offs?

Product Line:
AK5 Busbar System - GIC Product

Environment:
US Product

Cause:
Product Characteristics

Resolution:
The AK5 system has tap-offs included, but these require a specific AK5 socket for interface.  Reference the associated literature for this product as the entire unit is a system which requires compatible pieces to be used together.
Was this helpful?
What can we do to improve the information ?