Technical FAQs

Ask a Question

Shrouds with Power Distribution Lugs on GS Type Disconnect Switches

Issue:
Can the terminal shrouds for the GS1 and GS2 disconnect switches be used with distribution blocks?

Product Line:
IEC Disconnect Switches - GIC Product

Environment:
US Product

Cause:
Product Compatibility

Resolution:
The terminal shrouds are only designed to work with the standard terminal lugs.  These shrouds will not fit and are not to be used with the power distribution lugs.
Was this helpful?
What can we do to improve the information ?