Technical FAQs

Ask a Question

Add-on Poles for Smaller VLS Switches

Issue:
Are add-on poles available for VLS switches 16-32A?

Product Line:
IEC Disconnect Switches - GIC Product

Environment:
US Product

Cause:
Product Specification

Resolution:
The 40A add-on poles are suitable to be mounted and used on the 16A-40A switches.  For a standard simultaneous closing pole, use the following selection:

VLS3P016R1 - VLS1P040R1S
VLS3P025R1 - VLS1P040R1S
VLS3P032R1 - VLS1P040R1S
VLS3P016D1 - VLS1P040D1S
VLS3P025D1 - VLS1P040D1S
VLS3P032D1 - VLS1P040D1S
 
Was this helpful?
What can we do to improve the information ?