Technical FAQs

Ask a Question

Is the Local/Remote button on the VW3A1111 keypad functional when used with an ATV320 drive?

Issue:
Is the Local/Remote button on the VW3A1111 keypad functional when used with an ATV320 drive?

Product Line:
ATV320

Environment:
All models

Cause:
Desire to switch to Local control temporarily

Resolution:
The ATV320 does not support the Local/Remote button on the VW3A1111 remote keypad (only ATV6xx/9xx and ATV340 are supporting it).
The solution for ATV320 + VW3A1111 is to assign the TK function to one of the Fn keys.
Was this helpful?
What can we do to improve the information ?