Technical FAQs

Ask a Question

NPN Version of Biometric Switch

Issue:
Is there a NPN version of the biometric switch as shown in the instruction sheet?

Product Line:
Biometric Scanner - GIC Product

Environment:
US Product

Cause:
Product Selection

Resolution:
Originally there were plans to launch an NPN version of the scanner and the instruction sheet was created with this possibility.  In the end, it was decided that demand was not sufficient for this unit and only the PNP version was made available.
Was this helpful?
What can we do to improve the information ?