Technical FAQs

Ask a Question

Is it possible to change the root directory of a web visualization in SoMachine?

Issue:
Is it possible to change the root directory of a web visualization?
The default is /usr/visu/, but I would like to put it onto the removeable SD card, which gets mounted at /sd0.


Product Range:
SoMachine Software

Resolution:
 The default path to the web visualization is configured/set inside the controller's firmware, so unfortunately it is not accessible.
Was this helpful?
What can we do to improve the information ?