Technical FAQs

Ask a Question

Can you use the old ATV21 keypad VW3A21101 on the ATV212 drives?

Issue:
Can you use the old ATV21 keypad VW3A21101 on the ATV212 drives?

Product Line:
ATV21 and ATV212

Environment:
All 

Cause:
Wants to use the old VW3A21101 keypad on the ATV212 drives

Resolution:
Its not suggested that you use the old VW3A21101 keypad on the ATV212 drives.  Use the VW3A1101 keypad and VW3A1102 bezel on the ATV212 drive. 
 
Was this helpful?
What can we do to improve the information ?