Technical FAQs

Ask a Question

8501X minimal contacts needed with 8501XT timing attachment

Issue:
Does the 8501X relay require instantaneous contacts to utilize an 8501XT timing attachment?

Product Line:
Control Relays - GIC Product

Environment:
US Product

Cause:
Product Specification

Resolution:
No, the 8501XT timing attachment only requires the 8501X frame.  This frame may have contacts, but it is not required for proper operation of the timed contact module.
Was this helpful?
What can we do to improve the information ?