Technical FAQs

Ask a Question

Where should the third terminal on the 50437 (or TA30) be wired to the TeSys T ?

Issue:
What terminals should we wire Z1 and Z2 to on the external ground sensor

Product Line:
Tesys T Motor Management Systems

Environment:
Tesys T products

Cause:
Wiring and Installation
 
Resolution:
We should wire to terminals 1 and 2 on the ground sensor, terminal 3 should be left unwired. 
Was this helpful?
What can we do to improve the information ?