Technical FAQs

Ask a Question

Where can I get the triangular key to open up the GT250 unit?

PLEASE NOTE:
This is only intended for qualified personnel with proper personal protective equipment.

Issue:
Triangular Key to access the GT (3 phase unit)

Product Line
GT100,GT250,GT500MV

Environment:
Applications where a commercial 3 phase grid tie inverter is used

Resolution:
The open up the compartment the key is a standard 7 mm triangle key. (Ex. Hoffman A-L35Y)

*You can find many dealers and distributors that have that key by doing a search online with the following part description "Hoffman A-L35Y or equivalent"
Was this helpful?
What can we do to improve the information ?