Technical FAQs

Ask a Question

S-Flex enclosed drives do they come standard with the remote mounted HMI display on the door?

Issue:
S-Flex enclosed drives do they come standard with the remote mounted HMI display on the door?

Product Line:
S-flex enclosed with mod D07

Environment:
All 

Cause:
Wants to add the remote HMI to the S-flex enclosed drive. 

Resolution:
No the remote HMI is not standard on the S-flex enclosed drives.  If you want to add this option you will need to add the option suffix D07 to the order. 
Was this helpful?
What can we do to improve the information ?