Technical FAQs

Ask a Question

ATV930 with Embedded Ethernet, using with Rockwell 5000- what tags are present?

Issue:
ATV930 with Embedded Ethernet, using with Rockwell 5000- what tags are present? 

Product Line:
 ATV930

Environment:
 Embedded Ethernet

Cause:
 n/a
Resolution:

France response: ATV9xxEDSS import into Rockwell’s Studio 5000 does not bring any tags suitable for controlling our drive.
Working with ATV9xx on Rockwell PLC’s is based on Generic Ethernet Module – after inserting it, you will get the Controller Tags linked to the selected assemblies.
Please follow the attached below example.

 
Was this helpful?
What can we do to improve the information ?