Technical FAQs

Ask a Question

Are the battery terminal covers for the Conext SW the same as the TR inverter/charger?

Issue:
Will the plastic terminal covers for the TR fit on the CSW battery terminals?

Product Line:
Conext SW, TR inverter/charger

Environment:
Battery terminal covers are lost or damaged

Cause:
The part number for the battery terminal covers is 0J-0295.  The lead time for them may sometimes become very long because they are a spare part, and not ordered very often.  If available, the battery covers for the TR inverter/charger could be used.

Resolution:
The covers for the Conext SW and the TR inverter/charger are cross-compatible.
 
Was this helpful?
What can we do to improve the information ?