Technical FAQs

Ask a Question

ATV61/71HC high horse power drives fan control board relay is clicking on and off what would cause this?

Issue:
ATV61/71HC  high horse power drives fan control board relay is clicking on and off what would cause this?

Product Line:
ATV61

Environment:
All 

Cause:
Fan control board  relay is clicking

Resolution:
fan control board is clicking 

check your 3 phase 480vac on X1 terminal of the fan control board. 

swap X1 and X4 to see if there is an external supply being applies to RO SO TO
Was this helpful?
What can we do to improve the information ?