Technical FAQs

Ask a Question

Cannot Communicate with 9065SP to Change the Settings

Issue:
9065SPxxx will not communicate with 9065SPD on network although both units are connected and powered.

Product Line:
Solid State Overload Devices with Communication - GIC Product

Environment:
US Product

Cause:
Product Installation/Troubleshooting

Resolution:
Have customer scan network first.  9065MPD unit will not communicate with any device until it has done a network scan.
 
Was this helpful?
What can we do to improve the information ?