Technical FAQs

Ask a Question

How do you set up a split screen to show motor speed and motor current on the ATV61 and ATV71 HMI display?

Issue:
How do you set up a split screen to show motor speed and motor current on the ATV61 and ATV71 HMI display?

Product Line:
ATV61 and ATV71

Environment:
All 

Cause:
Set up split screen 

Resolution:
Main Menu is the starting point
Go to Menu 6 Monitoring configuration 
Go to Menu 6.2 Monitor Screen Type
Choose your Display Screen type (Digital, Bar Graph or List)
For this example choose Digital 
Was this helpful?
What can we do to improve the information ?