Technical FAQs

Ask a Question

Will a Powerpact L-frame install in an LA400S or LA400AWK enclosure?

Issue:
Will a  Powerpact L-frame install in an LA400S or LA400AWK enclosure?

Product line:
Molded case circuit breakers

Environment:
Selection 

Cause:
Installation

Resolution:
The LA400S and LA400AWK  enclosures only accepts the legacy  LAL, LHL, and Q4L style breakers.  The  L600AWK enclosure is currently the only available enclosure
for the L frame Powerpact circuit breakers. .  

Keywords:  Circuit breaker enclosure, Powerpact, Legacy, LAL, LHL, Q4L, LDL, LGL, LJL, LLL, LRL, L-frame
Was this helpful?
What can we do to improve the information ?