Technical FAQs

Ask a Question

What is the part number for the Modbus TCP Field-bus Module for the Altivar Process Drive?

Issue:
What is the part number for the Embedded Modbus Ethernet Field-bus Module for the Altivar Process Drive?

Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)

Environment:
All serial numbers for Altivar Process Drive 

Cause:
Part number required to order part

Resolution:
Modbus TCP or Modbus over Ethernet is embedded on the Altivar Process Drive
No option card is required
Was this helpful?
What can we do to improve the information ?