Technical FAQs

Ask a Question

Can a DC coil be swapped into an AC 8501XO or XMO relay?

Issue:
Can an AC 8501X be made into a DC 8501XD? 

Product Line:
Control Relays - GIC Product

Environment:
US Product

Cause:
Replacement coil

Resolution:
No, the DC coils are larger than the AC coils and will not fit in an AC device. The AC coils also will not fit properly in a DC device. 
Was this helpful?
What can we do to improve the information ?