Technical FAQs

Ask a Question

Are Fusible Plug In I-Line Busway Units Lockable?

Issue:
Are Fusible Plug In I-Line Busway Units Lockable?

Product Line:
I-Line Busway and accessories sold and supported in the USA.

Environment:
Maintenance

Cause:
Lock out/Tag out

Resolution:
Yes, the handle will accept up to three padlocks with 3/8" (9 MM) diameter shackle.
Reference Page 13 of the attached Instruction Bulletin 4512398101 for directions and pictures of this. 


 
Was this helpful?
What can we do to improve the information ?