Technical FAQs

Ask a Question

What size wires do the terminals accept on the LTMR TeSys T motor management controller?

Issue:
Terminal Wiring Characteristics

Product Line:
TeSys T Motor Management Controller

Environment:
North American Products

Cause:
Installation 

Resolution:
The table below describes the characteristics of cabls that may be used to wire the terminals: 

 

Cable Type No. of Conductors Conductor Section
mm^2 AWG
Flexible (stranded) cable Single conductor  .2...2.5   24...14 
2 conductors  .2...1.5   24...16 
Solid cable Single conductor  .2...2.5   24...14 
2 conductors  .2...1.0   24...18 
Flexible (stranded) cable with insulated cable ends Single conductor  .25...2.5   24...14 
2 conductors  .5...1.5   20...16 
Flexible (stranded) cable with non-insulated cable ends Single conductor  .25...2.5   24...14 
2 conductors  .2...1.0   24...18 
Was this helpful?
What can we do to improve the information ?