Technical FAQs

Ask a Question

What are the repair parts for the DTU462DS, series F6? (may be shown as F06)

Issue:
Design repair parts

Product Line:
Double Throw Safety Switches

Environment:
Repair parts

Cause:
Maintenance

Resolution:
The repair parts for the DTU462DS, series F6 (F06) are as follows. No other parts are available. (NOTE: Descriptions below of ``left side`` and ``right side`` mean your left or right as you face the switch.)
-Left Side Line Base - 4056625550 (one each upper and lower. Order arc suppressor, load lugs, and wire assembly separately. NOTE: thermoplastic cam between right and left line base may also be required).
-Right Side Line Base - 4056625050 (one each upper and lower. Order arc suppressor, load lugs, and wire assembly separately. NOTE: thermoplastic cam between right and left line base may also be required).
-Thermoplastic Cam between Left and Right Line Bases - 4056702801.
-Line Base mounting screws - 4020515101 (requires 3 per line base).
-Arc Suppressor Assembly - 4056635550 (requires 1 per line base).
-Arc Suppressor mounting screw - 4020514501 (requires 1 per arc suppressor).
-Wire Assembly Line Base - 4056732650 (requires 1 per phase. Includes cable factory connected mechanical lug at one end and at other end a crimped connector. Use mounting screws of line and load lugs.)
-Line and Load Lug Assembly - 4025101652 ( or order kit part #CL0306F - includes 6 lugs)
-Line, Load Lug mounting screw - 4020514202
-Ground Lugs - 4025101652 (the switch comes with 3 ground lugs from the factory).
-Ground Lug mounting screw - 4020513503
-Switch Mechanism - 4056646950 (each for upper and lower).
-Linkage Assembly - 4056665350 (links together upper and lower switch mechanisms). Also replace linkage assembly rubber gaskets.
-Linkage Assembly Rubber Gaskets - 40503-228-01 (3 total required)
-Linkage Assembly mounting screws - 2299940562 (requires 4) and 2194900001(requires 2).
-Handle - 4056688850
-Lockplate - 4056689501
-Lockplate mounting screws - 2194900001 (requires 2).
Was this helpful?
What can we do to improve the information ?