Technical FAQs

Ask a Question

Why XCNA or XC inverter power production was low?

Issue:
One of the phase is out
 
Product Line:
XC or XCNA
 
Environment:
 
Cause:
One of the inline fuse F1-F3 blown, fan fault or Dew point setting

Resolution:
If you have this fuse 0J-515-9300 (1250A fuse) then replace it. If not, call us at 866-519-1470 option 3 & 3 to open a case so that we can dispatch FSE to take care of it or we can send you a fuse so that you can replace it yourself. Also if there is a fan fault, this will limit the power production at 10%. In addition, if there is a dew point fault, the inverter will limit it power production at 50%.
 
Was this helpful?
What can we do to improve the information ?