Technical FAQs

Ask a Question

What is the difference between the ABE7CPA31 and the ABE7CPA31E?

Issue:
Can you explain the difference between the ABE7CPA31 and the ABE7CPA31E?

Product Line:
PLC

Environment:
Telefast
PLC
Remote block
ABE7

Resolution:
The ABE7CPA31 has screw terminals for the field connections and the ABE7CPA31E has spring terminals.

The ABE7CPA31 has screw terminals and the ABE7CPA31E is using spring terminals.
Was this helpful?
What can we do to improve the information ?