Technical FAQs

Ask a Question

What is the "C" Suffix on the Altivar 930 drives?

Issue:
What is the "C" Suffix on the Altivar 930 Drives?

Product Line:
Altivar 930 Process Drive (ATV930)

Environment:
All serial numbers for Altivar 930 Process Drive

Cause:
N/A

Resolution:
The "C" suffix designates that the drive does not have an internal braking transistor

Related FAQ:
FA304858: Do the Altivar Process Drives have integrated Braking Transistors?

 
Was this helpful?
What can we do to improve the information ?