Technical FAQs

Ask a Question

What's the maximum number of Sercos axis that the LMC078 can support?

Issue:
What's the maximum number of Sercos axis that the LMC078 can support?

Product Line:
LMC078

Resolution:
With the new hardware reference version RS02 (HW Code 0224013000000000) the number of supported axis by the LMC078 controller is now 24 axis (instead of 12 axis) in 4 ms.
Was this helpful?
What can we do to improve the information ?