Technical FAQs

Ask a Question

Why does my MPPT60-150 say I need to equalize my battery bank?

Issue:
Why is my MPPT60 displaying an “Equalize Due" message?

Product Line:
Conext MPPT60-150 865-1030-1

Environment:
Product Information


Resolution:
Equalize reminder should be set correctly
Reminder can be set anywhere from 0 to 365 days

Cause:
Charge controller has no way of knowing when the battery bank should be equalized, besides the user-input values

Please consult with the battery manufacturer for further information on battery maintenance
Was this helpful?
What can we do to improve the information ?