Technical FAQs

Ask a Question

Why am I not seeing the XW+ solar inverter on my System Control Panel?

Issue:
Customer is working on a new installation with a new inverter – XW+6848/5548 with an older System Control Panel (SCP)

Product Line:
Conext System Control Panel 865-1050

Environment:
Installation process


Resolution:
Upgrade the firmware on the SCP
Firmware can be found on http://solar.schneider-electric.com/

Cause:
Firmware on the older SCP needs to be upgraded to be compatible with the inverter's newer firmware
Was this helpful?
What can we do to improve the information ?