Technical FAQs

Ask a Question

What PV disconnect do I use on my MPP80 solar charge controller?

Issue: PV disconnect needs to be external from the SE PDP because the PDP is not rated for high voltage

Product Line: MPPT80 865-1032

Environment: Product Characteristics, installation support


Resolution: We offer a PV disconnect that is produced by Square D
SQUARE D HU361RB 30A 600V 3P 3Ph N3R Non-Fused / SQUARE D H361RB N 30A 600V 3PH FUSED NEMA 3
Was this helpful?
What can we do to improve the information ?