Technical FAQs

Ask a Question

How do I erase the password in my HMIGTO?

Issue:
I forgot the password for my HMIGTO. How to I delete security settings?

Product Line:
HMI Magelis

Environment:
This solution applies to the Magelis HMIGTO line.

Resolution:
The only way to delete security settings is to download another application to the HMIGTO using the SD card method.
In the Target Download property select "File System".
The Path property will be the drive letter of your SD card in your PC.
Right click on Target and choose "Download to file system"
Once complete insert the SD card in the HMIGTO SD card slot and power up.
The new application will be loaded from the SD card.
Was this helpful?
What can we do to improve the information ?