Technical FAQs

Ask a Question

Does Combox work with Insight Portal Through Mobile Hotspot?

Issue:

User wishes to connect the Combox via Mobile Hotspot to Insight Portal

Environment:
 
Conext Series / Combox

Resolution:

Combox will update via Mobile Hotspot to Insight Portal, as long as the Combox has internet source connection
Combox can be locally monitored without internet via connecting to the router.

Cause:
N/A
Was this helpful?
What can we do to improve the information ?