Technical FAQs

Ask a Question

Can you tell me what the limit is for TCP connections to the Ethernet port on the M340?

Issue:
How many connections does the Ethernet port on the M340 support?

Environment:
M340

Resolution:
The BMXP3420x0 CPUs support the following number of connections using port 502 messaging:
- servers (32 connections)
- clients (16 connections)
-  Transparent Device Access (2 connections)
Was this helpful?
What can we do to improve the information ?