Technical FAQs

Ask a Question

XW Series Inverter Compliance with NEC 690.12 Rapid Shutdown

Issue:
XW Series Inverter does not come with Emergency Disconnect Switch that is compliant with NEC 690.12 Rapid Shutdown Requirement 

Product Line:
XW Series Inverter

Environment:
XW Series Inverter Solar System Rapid Shutdown 

Cause:
In certain scenarios, XW Series Inverter is required to be compliant with NEC 690.12 Rapid Shutdown Requirement. 

Resolution:

MidNite Solar Products provide Emergency Disconnect Switch that can be installed with XW Series Inverter to be compliant with NEC 690.12 Rapid Shutdown Requirement. 

http://www.midnitesolar.com/products.php?menuItem=products&productCat_ID=44&productCatName=RAPID-SHUTDOWN-SYSTEM-NEC-690.12
Was this helpful?
What can we do to improve the information ?