Technical FAQs

Ask a Question

Wanted a 3 contactor Bypass on the ATV660 enclosed package.

Issue:
Wanted a 3 contactor Bypass on the ATV660 enclosed package.

Product Line:
ATV660 

Environment:
Bypass selection

Cause:
n/a

Resolution
Richard Jennens response: 75 HP and below, the closest equivalent is the 2 contactor with disconnect switch option. 3-contactor is available 100 HP and above.
3-contactor bypass for 75HP and below is a Drives Quote Group custom solution.
 
Was this helpful?
What can we do to improve the information ?