Technical FAQs

Ask a Question

VBF4 Mounting Screws

Issue:
What size mounting screws are used with the VBF4 and are they included with the part?

Product Line:
Vario Switches - GIC Product

Environment:
US Product

Cause:
Product Specifications

Resolution:
The VBF4 comes with four Phillips head M3.5 X 16mm steel screws.
Was this helpful?
What can we do to improve the information ?