Technical FAQs

Ask a Question

I can read from my STBNIP2311 island but can't write to it.

Issue:
I get error 3002 when I try to write to my Advantys STB drop.

Product Line:
Advantys STB

Resolution:
If the STBNIP2311 is using the default IP address you can not write to it. You can only read from it.
You will get Modbus error 3002.
Was this helpful?
What can we do to improve the information ?