Technical FAQs

Ask a Question

Are Other Accessories Necessary to use the XB5 Biometric Switch with USB?

Issue:
Is any other equipment needed with the XB5 Biometric switches?  Does the USB need to be connected to anything else for the Biometric Switch to work?

Product Line:
Biometric Switches - GIC Product

Environment:
US Product

Cause:
Product Selection

Resolution:
These units are designed  stand alone.  The USB connection is optional for connecting to a computer and transferring a database of users with XB5 Soft.  No other accessories are strictly needed for setup.
Was this helpful?
What can we do to improve the information ?